Part Number: LAUNCHXL2-RM57L
Tool/software:
Hi,
I am building a setup for characterization of a sensor which outputs the sensed value of a physical parameter in the form of a current which is in the range of microamperes. The range can be anywhere between 5uA - 30uA.
As far as I understand, I need to convert this current into voltage before giving it (as an input) to ADC on RM57L-Launchpad converts voltages to digital values. I want to know exactly how do I do this? Can I just keep a 1MΩ resistor and tap the voltage across it as an input to the ADC module or use a transimpedance amplifier whose output can be given to ADC?
If transimpedance amplifier is the answer, does TI offer any such ICs that do this?
Regards,
Chetan.