Part Number: TMS570LC4357
Tool/software:
Hi,
Inorder to generate delay, we have the following pseudo code, which is similar to an example code from TI
period_value refers to the amount of delay needed(passed as an argument).
When the controller is running continuously for days, is there any chance that, current_time value will be less than initial_time value because of roll over condition of uint64 type. The question is, if roll over occurs for the above variables, how the handling is done in TI ? or should we add any rollover conditions in the code ?