Part Number: TMS570LC4357
Tool/software:
Hi
I downloaded the 80MHz HCLK example from the related thread and was able to program the flash.
Now, I want to be able to program the flash without using the Fapi_issueProgrammingCommand() APIs, so I followed the instructions in SPNA148. I could not get that to working. Attached is the screenshot of the code that does not work.
But if I replace the highlighted statement with below statement, it works fine and programs the locations specified for Bank 7.
Return_Status = Fapi_issueProgrammingCommand((uint32_t*)FL_PROG_ADDR_B7,DataBuffer,8,0,0,Fapi_AutoEccGeneration);
This tells me there is something that "Fapi_issueProgrammingCommand" function performs that I do not understand. Any suggestions please?
Thank you.