Part Number: AM2432
Tool/software:
hello:
excuse me, there are two questions
1、Why can't the AM243 use USB peripherals when booting in DEV MODE?
2、My custom PCB board currently doesn't have UART pin, so I can not " Flash SOC Initialization Binary" using the serial port. I booting the chip in DEV MODE and running the script on CCS, I can run the program, but the USB peripherals don't work. When I previously tested with the evm, I found that the USB peripherals worked in xspi mode. How should I proceed with this?
thanks