Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU-PLUS-SDK-AM243X: Rx pin configuration via SysConfig

Part Number: MCU-PLUS-SDK-AM243X

Tool/software:

I have a question concerning the TI System Configuration Tool. When I select my peripherals to generate the pinmux settings, there is a "Rx" option for each pin. What does that option represent?

Here is a screenshot to illustrate what I'm talking about:

For the GPMC, all the pins should be bidirectional. Should it not be configured as RX?

Thanks!

  • Hello Eden,

    For the GPMC, all the pins should be bidirectional. Should it not be configured as RX?

    Actually, for the GPMC NAND interface, AD0 to AD7 lines are only data lines and all are input to SOC.

    And there are no address line concept for NAND memories, and it is just command and read based-methodology for NAND memories.

    For example, we need to read data one page approximately 4KB and the page size will be different based on vendor.

    Now, from the SOC side, we need to send an address command which includes some of the row and column selections and after that NAND devices will send data to SOC.

    This is how NAND memory works . In this method, all data lines are input to SOC. So, it enabled RX. 

    When you enable RX - >, Pin should be configured as input.

    If you look at the datasheet of AM64X for GPMC_ADO pin, and it supports both Input and output.

    But in NAND device interface type, it can be used only as input and that's reason it was configured as RX mode.

    Regards,

    Anil.

  • Ok so if I want to configure a pin as bidirectional, I need to NOT select RX mode? As in, if it's specifically an input and input only I select the Rx option, and I deselect it if it's an output or bidirectional?

  • Hello Eden,

    Don't select the Rx signal and see if it works.

    In this set up we just set up Mux mode operation and by default it will be configured as output if we do not enable input mode.

    May I know which memory (NAND or NOR or PSRAM or FPGA )  did you connect ? 

    Regards,

    Anil.