Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1106: UART boot support in BSL and 'BSL_invoke' input signal?

Part Number: MSPM0L1106
Other Parts Discussed in Thread: MSPM0L1306

Tool/software:

Team,
Can you please confirm the below?

We want to use the internal bootloader of an MSPM0 to load our application via the internal UART later in production:
Refering to
   MSPM0 Bootload UG - slau887:

   MSPM0L1306 datasheet SLASEX0
Do I understand correctly that if the MCU is un-programmed (see slau887 section 3.2.1)

,then we no longer need a BSL_invoke input signal (slau887 Figure 3-2)?

SLASEX0 MSPM0L1306 Datasheet section 8.27:

Thanks in advance,

ANthony

  • o I understand correctly that if the MCU is un-programmed (see slau887 section 3.2.1)

    Yes, if the main flash is empty the device will to into BSL automatically, but there is a 10 seconds time out feature, you need to communicate with the device within 10s or it will to into standby.