Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000-CGT: F2800137 uint8_t option

Genius 3186 points

Part Number: C2000-CGT

Tool/software:

Hello,

May I have question about CCS project and C2000 compiler for F280013x?

I want to use uint8_t (because sample for reference designe is using this).

but it seems only uint8_t/int8_t is disable in _stdint.h that define uint*_t .

Is this can change to enable by compiler setting?

If yes, could you tell me which setting?

Thanks,

GR