Part Number: TM4C123GH6PM
Tool/software:
Hello,
I'm trying to write a code that measures the voltage through PC6 and see if it exceeds the reference voltage that I set in the code. My code is shown below and the reference voltage is 0.1375V. When I adjust voltage through the DC power supply (+ terminal connected to PC6 and ground terminal is connected to TM4C's ground), nothing really happens or changes from the initial state. How should I fix my code so that whenever the voltage is below the reference voltage, the RED LED turns off, and when it is above, the RED LED turns on? Also, I think I've correctly updated the vector table for the interrupt.
#include <stdint.h>
#include <stdbool.h>
#include <string.h>
#include "inc/tm4c123gh6pm.h"
#include "inc/hw_memmap.h"
#include "inc/hw_gpio.h"
#include "driverlib/pwm.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/ssi.h"
#include "driverlib/adc.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include "driverlib/interrupt.h"
#include "driverlib/comp.h"
void Comparator0IntHandler(void);
void Comparator_Init(void);
void Comparator_Init(void)
{
// Enable the peripherals for the comparator and GPIO
SysCtlPeripheralEnable(SYSCTL_PERIPH_COMP0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
// Configure the comparator input pin (e.g., C0+ on PC6)
GPIOPinTypeComparator(GPIO_PORTC_BASE, GPIO_PIN_6);
// Configure the internal reference for the comparator
ComparatorRefSet(COMP_BASE, COMP_REF_0_1375V); // Use the closest available reference voltage
// Configure the comparator
ComparatorConfigure(COMP_BASE, 0, COMP_TRIG_NONE | COMP_INT_BOTH | COMP_ASRCP_REF);
SysCtlDelay(100);
// Clear any pending comparator interrupts
ComparatorIntClear(COMP_BASE, 0);
// Enable comparator interrupt
ComparatorIntEnable(COMP_BASE, 0);
// Enable the interrupt in the NVIC (Nested Vectored Interrupt Controller)
IntEnable(INT_COMP0);
IntMasterEnable();
}
void Comparator0IntHandler(void)
{
// Clear the comparator interrupt
ComparatorIntClear(COMP_BASE, 0);
// Handle the comparator output (you can add your logic here)
if (ComparatorValueGet(COMP_BASE, 0))
{
// Voltage is above the threshold
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, GPIO_PIN_1); // Turn on the RED LED
// UARTprintf("high");
}
else
{
// Voltage is below the threshold
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0); // Turn off the RED LED
// UARTprintf("low");
}
}
void main(void)
{
// Set the system clock to 80 MHz
SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
// Enable the GPIO port for an LED (for demonstration purposes)
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1);
// Initialize the comparator
Comparator_Init();
while (1)
{
}
}