Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL2-RM46: TM4C129ENCPDTI384A3RCWG4

Part Number: LAUNCHXL2-RM46
Other Parts Discussed in Thread: TM4C129ENCPDT, UNIFLASH, TMDSEMU110-U, TM4C1294NCPDT,

Tool/software:

I am working with a TELIT CINTERION cellular module (LE910C1_EU) and I want to use the FOTA of this module to update my micro and I have the following questions:

¿Es posible obtener las librerías en C del JTAG XDS110 para cargarlas e instalarlas en el micro TM4C129ENCPDT?, el cuál actuará como compilador de mi micrcontrolador principal (RM46). Is it possible to get the C libraries from the XDS110 JTAG to load and install them on the TM4C129ENCPDT micro, which will act as a compiler for my main microcontroller (RM46)?

For USB communication between the processor (PC) and the TM4C129ENCPDT microcontroller, are specific USB drivers required or are they standard?

  • Hi,

      Refer to the XDS110 Debug Probe User's Guide https://software-dl.ti.com/ccs/esd/documents/xdsdebugprobes/emu_xds110.html and go to Updating the Firmware section. 

    Updating the Firmware

    Automatic update

    When using ccsv8.1.1+ or ccsv8.1.0 with TI Emulators package version 6.0.14.5 or newer, the firmware on the XDS110 is updated automatically when connecting from inside CCS.

    Note that the firmware is not automatically reverted to a prior version unless there's been a major change. For most scenarios, all changes are backwards compatible to ensure this works. If a change is needed that is not backwards compatible, then the major version numbers will change as a flag that it can't work.

    Examples:

    • CCS supports firmware 2.3.0.12, XDS110 has firmware 2.3.0.8 → XDS110 will be updated to 2.3.0.12
    • CCS supports firmware 2.3.0.12, XDS110 has firmware 2.3.0.14 → XDS110 will not be reverted
    • CCS supports firmware 2.3.0.12, XDS110 has firmware 2.4.0.1 → XDS110 will be reverted to 2.3.0.12

    Note:

    The firmware update process prompts the user when it is detected when launching a debug session in CCS, Uniflash and in other utilities such as SmartRF Studio or SmartRF Flash Programmer. When using the Test Connection button or the command line utility <dbgjtag.exe>, the update happens without prompting.

    Manual update

    If manual updating or diagnostics is required, using a Windows host is highly recommended. Close any instances of CCS that are running in your system. Open a Windows Command Prompt and issue the following commands:

    Note:

    The steps below are for an installation of CCSv10.4 in the default directory. Please update the path and firmware file name when using different CCS and firmware versions.

    Note:

    For UniFlash, the path to the XDS110 folder is: [UNIFLASH INSTALL DIR]\deskdb\content\TICloudAgent\win\ccs_base\common\uscif\xds110.

    1. Go to the directory where the utility is installed:

    C:\>cd C:\ti\ccs1040\ccs\base\common\uscif\xds110

    2. Run the configuration just to make sure a XDS110-class debugger is connected (or to list how many are connected) and what is the firmware revision installed on it:

    C:\ti\ccs1040\ccs\base\common\uscif\xds110>xdsdfu -e

    3. Put the XDS110 in DFU mode:

    C:\ti\ccs1040\ccs\base\common\uscif\xds110>xdsdfu -m

    4. Run the updater, passing the firmware file and resetting the debug probe afterwards:

    C:\ti\ccs1040\ccs\base\common\uscif\xds110>xdsdfu -f firmware_3.0.0.16.bin -r

    In case of a bricked pod

    In certain scenarios there is a chance your Pod or Launchpad becomes bricked by the firmware update. Check the Troubleshooting section below for additional details.

    Finding and updating the serial number

    When using multiple debug probes in the same host, in general it is necessary to properly differentiate each debug probe by serial number.

    To find out what is the serial number of all connected debug probes, follow steps 1 and 2 above

    If you want to set the serial number to a specific value:

    1. Unplug all other debug probes from the host

    2. Follow steps 1 through 3 above

    3. Set the serial number suffix (RECOMMENDED):

    C:\ti\ccs1040\ccs\ccs_base\common\uscif\xds110>xdsdfu -n 4567 -r

    Notes:

    The -n option preserves the prefix of the serial number, which allows the board to make use of the Autodetect feature. See this short youtube clip for details.

    To set the entire serial number, use the option -s followed by an 8-digit unique number.

    Additional details are also described in the document:

    [CCS INSTALL DIR]\ccs\base\common\uscif\xds110\XDS110SupportReadMe.pdf

    Serial Number restrictions

    Serial numbers for the XDS110 must be 8 characters long and consisting of only printable ASCII characters that is not a comma (ASCII HEX: 0x2C). It is recommended to use only alphanumeric characters for best compatibility.

    IMPORTANT!

    As of June/2018, the standalone XDS110 Debug Probe (TMDSEMU110-U) requires an update to the bootloader to allow recording the serial number. To do that, issue the following commands before updating the serial number:

    C:\ti\ccs1040\ccs\base\common\uscif\xds110>xdsdfu -m

    C:\ti\ccs1040\ccs\base\common\uscif\xds110>xdsdfu -b boot_loader.bin -r

  • Thank you for your response.

    1º: For my application I am not going to use the product "TMDSEMU110-U" because the goal is to develop my own debugger that will go on my PCB, so I want to know if the steps described in your answer would be the same for any other microcontroller.

    2º: I want my microcontroller to be used for other functions and not only for debugging, so I would like to know if you provide the source code for the file "xdsdfu -f firmware_3.0.0.16.bin -r".

    3º: I realised that for my application I don't need the debugging part. It would be enough with the process of running the boatlader as explained in these tutorials: https://www.ti.com/lit/an/spna183/spna183.pdf

    https://www.ti.com/lit/an/spna189/spna189.pdf?ts=1719743482175&ref_url=https%253A%252F%252Fwww.google.com%252F

  • 1º: For my application I am not going to use the product "TMDSEMU110-U" because the goal is to develop my own debugger that will go on my PCB, so I want to know if the steps described in your answer would be the same for any other microcontroller.

    For the onboard XDS110, tt would have to be based on a supported device like the TM4C1294NCPDT

    2º: I want my microcontroller to be used for other functions and not only for debugging, so I would like to know if you provide the source code for the file "xdsdfu -f firmware_3.0.0.16.bin -r".

    We do not provide the source code for the firmware

    3º: I realised that for my application I don't need the debugging part. It would be enough with the process of running the boatlader as explained in these tutorials: https://www.ti.com/lit/an/spna183/spna183.pdf

    I would need the device experts to comment on this.

    Thanks

    ki

  • 1º: As I mentioned earlier in the post, I am working with the LAUNCHXL2-RM46, so I need a list of compatible devices to be able to perform the steps described in the previous answer.

    2º:I am sad to know this because it is a limitation for developers and programmers. Even with this limitation, is there any way I can use my microcontroller for other functions and not only for debugging?

    3º:I would like you to discuss this issue with your expert as this information I have passed on to you is explained by a famous TI_GURU as "QJ Wang".

    I would like your answers to give some detailed solutions to my questions and not just short statements. Thank you

  • Hi Jaun,

    3º: I realised that for my application I don't need the debugging part. It would be enough with the process of running the boatlader as explained in these tutorials: https://www.ti.com/lit/an/spna183/spna183.pdf

    The XDS debuggers that will provide on Launchpad's or HDK boards are for easy debugging purpose only. You don't need to include these XDS emulator IC's in your PCB board for mass production.

    Please refer below thread from QJ:

    (+) WEBENCH® Tools / TMDX570LC43HDK : Can I get the CPLD source of TMDX570LC43HDK? - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

     So, what customers will do is that they will remove these XDS emulator IC's in their final custom board and instead of this they will provide a provision for 20-pin ARM JTAG connector for direct code flashing into the Hercules controllers. So, we don't provide the source code of XDS emulators to the customers for their customization because they will be used only on our TI-specific Launchpad or HDK boards and not for end products.

    So, if you want to use UART or CAN or Ethernet or SPI etc. bootloaders in your application then you should need to place them in the starting sectors of the flash only and on top of that you can place your main application like QJ described in his application notes.

    CAN Bus Bootloader for RM46 MCU (ti.com)

    UART Bootloader for Hercules RM46 MCU (ti.com)

    --
    Thanks & regards,
    Jagadish.

  • 1º: As I mentioned earlier in the post, I am working with the LAUNCHXL2-RM46, so I need a list of compatible devices to be able to perform the steps described in the previous answer.

    TM4C1294NCPDT and MSP432E401YTPDT (both 128 pin) are compatible for any XDS110 design.

    2º:I am sad to know this because it is a limitation for developers and programmers. Even with this limitation, is there any way I can use my microcontroller for other functions and not only for debugging?

    What is the goal of obtaining the XDS110 source code? Do you wish to modify the XDS110 firmware so that you can use the XDS110 device for other things than just XDS110 debug?

  • Yes, this has been one of the questions from the beginning of the post, to get the C libraries from the XDS110 JTAG to load and install them in the TM4C129ENCPDT micro, which will act as compiler for my main microcontroller (RM46). So the goal is to get the source code so that the TM4C129ENCPDT microcontroller doesn't act only as a debugger and can be used for other functions.

  • Hi @Ki,

    Will you provide the response, whether it is possible to provide source code for TM4C129ENCPDT or not?

    --
    Thanks & regards,
    Jagadish.

  • I am waiting for an answer. Thank you

  • Sorry, we do not support custom modifications of the XDS110 firmware. This also means that we do not provide the source code for it.

  • Is there no way I can use my microcontroller as a debugger, and still use this microcontroller for other functions, such as developing my own code? I mean, can I put the binary code from the XDS110 into the microcontroller and still use it?

  • Is there no way I can use my microcontroller as a debugger, and still use this microcontroller for other functions, such as developing my own code?

    It may be possible but we do not support this scenario.

  • If Texas Instruments does not support this problem, who does? Because the problem of not getting information from the binary file is being imposed on me by Texas Instruments