This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G1505: External PWM max input frequency at TIMx

Part Number: MSPM0G1505

Tool/software:

Hi, 

I would like to input an external PWM frequency of 400kHz into this device using TIMx input capture.

I have looked through MSPM0G1505 datasheet to identify the maximum input frequency at TIMx I/O pin and found this table below. 

Since it mentions "port output frequency", can I confirm that this max frequency details for both input/output ports, hence there is no issues on feeding TIMx port an external PWM of 400kHz?