Part Number: AM2634-Q1
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Dear Champs,
My customer is looking for some ADC example implementing internal reference without HW ADC_VREF pin connected as in below.
Is there any example to use internal reference?
Internal reference are disabled by default. If external reference is not used, internal reference buffers can be enabled by the application for driving the ADC reference. The ADC_REFBUF0_CTRL register is used to enable ADC Reference Buffer 0. Similarly, the ADC_REFBUF1_CTRL register is used to enable ADC Reference Buffer 1. The MASK_ANA_ISO register must be set to 0x7 before ADC reference buffers are enabled. This prevents any undesirable behavior from voltage monitors triggering SOC reset.
Thanks and Best Regards,
SI.