Part Number: MCU-PLUS-SDK-AM243X
Tool/software:
Hi team,
 
 We uses AM243x_lp to build a custom flash ic board integrating an OSPI-Flash from Macronix. The flash used is the MX25L25645GM2I-08G.The SDK version I am using is mcu_plus_sdk_am243x_09_00_00_35.
I replaced the LP-AM243's external flash with an MX25L25645GM2I-08G.I checked the SDK instructions and found an article on how to apply custom flash to the LP. 
 Based on that, I attempted to update the flash parameters using our chosen flash data sheet and the.json file included with the SDK. 
 I've attached the. Json file for the MX25L25645GM2I-08G flash IC. Have the MX25L25645G settings been setup correctly in this. Json file?
{
    "flashSize": 33554432,
    "flashPageSize": 256,
    "flashManfId": "0xC2",
    "flashDeviceId": "0x2018",
    "flashBlockSize": 262144,
    "flashSectorSize": 4096,
    "cmdBlockErase3B": "0xD8",
    "cmdBlockErase4B": "0xDC",
    "cmdSectorErase3B": "0x20",
    "cmdSectorErase4B": "0x21",
    "protos": {
        "p111": {
            "isDtr": false,
            "cmdRd": "0x03",
            "cmdWr": "0x02",
            "modeClksCmd": 0,
            "modeClksRd": 0,
            "dummyClksCmd": 0,
            "dummyClksRd": 15,
            "enableType": "0",
            "enableSeq": "0x00",
            "dummyCfg": null,
            "protoCfg": null,
            "strDtrCfg": null
        },
        "p112": null,
        "p114": {
            "isDtr": false,
            "cmdRd": "0x15",
            "cmdWr": "0x02",
            "modeClksCmd": 0,
            "modeClksRd": 0,
            "dummyClksCmd": 0,
            "dummyClksRd": 8,
            "enableType": "5",
            "enableSeq": "0x00",
            "dummyCfg": null,
            "protoCfg": null,
            "strDtrCfg": null
        },
        "p118": null,
        "p444s": null,
        "p444d": {
            "isDtr": true,
            "cmdRd": "0xED",
            "cmdWr": "0x02",
            "modeClksCmd": 0,
            "modeClksRd": 1,
            "dummyClksCmd": 0,
            "dummyClksRd": 15,
            "enableType": "0",
            "enableSeq": "0x08",
            "dummyCfg": {
                "isAddrReg": true,
                "cmdRegRd": "0x65",
                "cmdRegWr": "0x71",
                "cfgReg": "0x00800003",
                "shift": 0,
                "mask": "0x0F",
                "bitP": 15
            },
            "protoCfg": null,
            "strDtrCfg": null
        },
        "p888s": null,
        "p888d": null,
        "pCustom": null
    },
    "addrByteSupport": "1",
    "fourByteAddrEnSeq": "0xA1",
    "cmdExtType" : "NONE",
    "resetType": "0x10",
    "deviceBusyType": "1",
    "cmdWren": "0x06",
    "cmdRdsr": "0x05",
    "srWip": 0,
    "srWel": 1,
    "cmdChipErase" : "0xC7",
    "rdIdSettings": {
        "cmd": "0x9F",
        "numBytes": 3,
        "dummy4": 0,
        "dummy8": 0
    },
    "xspiWipRdCmd": "0x00",
    "xspiWipReg": "0x00000000",
    "xspiWipBit": 0,
    "flashDeviceBusyTimeout": 6000000,
    "flashPageProgTimeout": 4000
}
1. Got a load failed error while debugging.
MAIN_Cortex_R5_0_0: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x40: (Error -1065 @ 0x40) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 12.6.0.00029) 
MAIN_Cortex_R5_0_0: File Loader: Verification failed: Target failed to write 0x00000000
MAIN_Cortex_R5_0_0: GEL: File: C:\Users\Abinaya.e\Downloads\Macronix_flash_diag_am243x-lp_r5fss0-0_nortos_ti-arm-clang\Macronix_flash_diag_am243x-lp_r5fss0-0_nortos_ti-arm-clang\Debug\Macronix_flash_diag_am243x-lp_r5fss0-0_nortos_ti-arm-clang.out: Load failed.
 
 
   2. 2. Also, when I attempted to flash the code in UART flash mode according to the flash guide LINK  , it halted in the second instruction. (--operation=flash-phy-tuning-data)
 
Could you kindly advise me on the reason of the problem and how to fix it?
Regards,
Abinaya