Part Number: MSPM0L1306
Other Parts Discussed in Thread: MSP430FR2476,
Tool/software:
I would like to know which of the external clock input pins, MSPM0L1306 or MSP430FR2476, is more resistant to noise.
The external clock is 40kHz,
MSPM0L1306: PA14/TIMG1.CCP0
MSP430FR2476: P1.6/TA1CLK
The pins for the external clock are set as above.
When comparing the MSPM0L1306 and MSP430FR2476, is there any reason or basis for saying that the MSPM0L1306 has higher noise resistance, for example, the MSPM0L1306 pins have lower input impedance and are less susceptible to noise, or the input capacitance is lower and therefore less susceptible to noise?