Part Number: MCU-PLUS-SDK-AM243X
Tool/software:
Hi, Experts
I have problems at below URL with initializing our custom board.
SBL NULL is loaded as shown below.

Before running loadJSFile "load_dmsc_hsfs.js", I initialized DDR with GEL file, so I waited it indefinitely.
However, after running this, I initialized DDR, and I got the log as below.

full log :
MAIN_Cortex_R5_0_0: GEL Output: --->>> DDR4 Initialization is in progress ... <<<---
MAIN_Cortex_R5_0_0: GEL Output: --->>> ECC Disabled <<<---
MAIN_Cortex_R5_0_0: GEL Output: --->>> DDR controller programming in progress.. <<<---
MAIN_Cortex_R5_0_0: Trouble Writing Memory Block at 0x5f8 on Page 0 of Length 0x4: (Error -1170 @ 0x5FC) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 12.7.0.00105)
AM24_DDR_Initialization_ECC_Disabled() cannot be evaluated.
Target failed to write 0x000005F8
at *((unsigned int*) (AM24_DDRSS_CTL_BASE+0x5f8))=(unsigned int) 0x00000000 [AM24_DDRSS_Config.gel:34]
at DDRSS_Init_Reg_Copy(0) [AM24_DDRSS_Config.gel:129]
at AM24_DDR_Initialization_ECC_Disabled()
What should I do?