Part Number: MSPM0L2228
Tool/software:
Hello Expert
The power supply voltage of MSPM0L2228 is 3.3V, so when driving an LCD, it is also a 3.3V LCD. May I ask if it can support a high contrast ratio of 2000:1.
Currently, we have designed 20 segments and 3 MUXS PINs,
1.If it cannot support a contrast of 2000:1, what is the maximum contrast that can be supported.
2. Can we increase contrast by reducing MUXS pins, such as changing to 2 MUXS pins and 30 segments, and what is the maximum contrast that can be achieved?
3.Is there any other way to improve contrast?
Thank you.
BR
Alex Xu