Part Number: MSPM0G3107
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
I am trying to setup input capture for a timer in sysconfig, but do not see the right pin listed.
I am using mspm0 3107 32 pin package and according to the 310x datasheet, PA16 should expose a timer input (see the screenshot below):

However, when I look it in the sysconfig, I do not see PA16 available (see the screenshot below):

Could you confirm whether I can use PA16 for input capture or I need to use a different basically pin ?
This change would require a schematic modification which is not ideal.
Thanks,
Mykola