Part Number: LP-MSPM0C1104
Tool/software:
Hi, experts:
I used CCS Theia 1.3.1 to set uart and PWM configuration of 20 WQFN in LP-MSPM0C1104, I set TIMA0 & TIMG14 as PWM output source, and PA26 as RX , PA23 as TX of uart, but I found the jumper of rxd between XDS110 and MCU has an impact on uart and PWM function, if I remove the jumper, PA26 can work as RX well, while PWM can't ouput, otherwise the opposite situation, I wonder if it is expected, I want to test the uart and PWM function at the same time to make sure everything works well, please help to check, thanks.
Bill