Tool/software:
Hi All,
We are using AM263x controller and in that we are on developing the custom CAN based bootloader (Basically UDS based) which will take the input over can from hex file and load into the memory and jump to the that particular core.
but currently there is SBL which will need to load the program every time once we debug it and once it is power ON reset then it is not jumping to the whatever software is flashed it need to again connect to the target and then Load program.
Is there any way to bypass the SBL and load Our Custom bootloader and it will invoke after every Power ON cycle.
Thanks in advanced,
Shriram Madhavai