Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0C1103: Flashing FW via I2C

Part Number: MSPM0C1103
Other Parts Discussed in Thread: MSPM0C1104,

Tool/software:

Hi,

can the MSPM0C1103 or MSPM0C1104 be flashed over I2C?

Thanks,

Marinus

  • Hi Marinus,

    Yes and no.  Yes, programming the MSPM0C via I2C is possible using bootloader, but no, the MSPM0C family does not come with installed bootloader in ROM, as does MSPM0L/G families.  Customer would need to compile/build bootloader in FLASH as part of their application.  The bootloader code is provided in the SDK.

  • Thank you Dennis,

    When using the MSPM0C*, do you know if it is possible to lock some part of the flash to make sure that the boot-loader won't be overwritten?

    Thanks,

    Marinus

  • Hi Marinus,

    The BSL source code is located in the SDK.

    Here is typical install directory -> C:\ti\mspm0_sdk_2_01_00_03\examples\nortos\LP_MSPM0C1104\bsl

    There is a readme.md file that describes the BSL and in there it mentions that the BSL is located in the first 6k of memory and is "static write protected" which means during a mass erase, the BSL is protected from erasure.

    I attached the readme.md for convenience.

    ## Example Summary
    
    * Flash BSL is developed to provide BSL features in a device not having ROM BSL.
    * The Memory Section is altered to achieve this.(refer mspm0c1104.cmd)
    * Flash Bootloader supports programming / verifying data in the memory.
    * It can be invoked in any of the three way as follows:
    	* No Application at APP START
    	* BSL PIN Inovation
    	* Application based invocation
    * It supports the following major functions
    	* Program data
    	* Get Device info
    	* Flash memory erase
    	* Readback data
    	* CRC verification
    	* Start Application
    * One of UART/I2C interface can be used to communicate with the Host.
    * By default flash BSL occupies the first 6 KB of flash.
    * This region is static write protected using bootcode user configuration. ( refer "boot_config.c" )
    * Once this image is loaded to the device, the FLash Bootloader will be active. To revert the device to default state SWD_Factory_Reset command has to be used.
    * Users can alter the interface pins/ invoke pin in bootloader user configuration (refer boot_config.c)
    * The user application is expected to start at 0x1800 by default.
    
    ## Flash BSL feature selection
    * The following features are Macro based and can be enabled/disabled to save memory consumption (refer "flashBSL_modules.h")
    	* UART_INTERFACE
    	* I2C_INTERFACE
    	* BSL_PIN_INVOKE
    	* BSL_BLANK_FLASH_INVOKE
    	* BSL_CMD_FLASH_RANGE_ERASE
    	* BSL_CMD_MASS_ERASE
    	* BSL_CMD_MEMORY_READ_BACK
    	* BSL_CMD_STANDALONE_VERIFICATION
    	* BSL_CMD_CHANGE_BAUDRATE
    	* BSL_CMD_GET_IDENTITY
    	* BSL_TIMEOUT
    
    NOTE:
    * By enabling/ disabling features, the RAM buffer size for BSL communication and Flash start address for Application are altered. The values are to be updated in `flash_bsl_defines.h` accordingly
    * While creating flash bootloader make sure that, flash bootloader is static write protected. Otherwise there are chances for device to get locked during the boot loading process.
    
    For more details on BSL communication interface refer to BSL User Guide.
    
    ## Peripherals & Pin Assignments
    
    | Peripheral | Pin | Function |
    | --- | --- | --- |
    | DEBUGSS | PA20 | Debug Clock |
    | DEBUGSS | PA19 | Debug Data In Out |
    
    
    ## BoosterPacks, Board Resources & Jumper Settings
    Visit [LP_MSPM0C1104](https://www.ti.com/tool/LP-MSPM0C1104) for LaunchPad information, including user guide and hardware files.
    
    | Pin | Peripheral | Function | LaunchPad Pin | LaunchPad Settings |
    | --- | --- | --- | --- | --- |
    | PA20 | DEBUGSS | SWCLK | N/A | <ul><li>PA20 is used by SWD during debugging<br><ul><li>`J101 15:16 ON` Connect to XDS-110 SWCLK while debugging<br><li>`J101 15:16 OFF` Disconnect from XDS-110 SWCLK if using pin in application</ul></ul> |
    | PA19 | DEBUGSS | SWDIO | N/A | <ul><li>PA19 is used by SWD during debugging<br><ul><li>`J101 13:14 ON` Connect to XDS-110 SWDIO while debugging<br><li>`J101 13:14 OFF` Disconnect from XDS-110 SWDIO if using pin in application</ul></ul> |
    
    
    ### Device Migration Recommendations
    This project was developed for a superset device included in the LP_MSPM0C1104 LaunchPad. Please
    visit the [CCS User's Guide](https://software-dl.ti.com/msp430/esd/MSPM0-SDK/latest/docs/english/tools/ccs_ide_guide/doc_guide/doc_guide-srcs/ccs_ide_guide.html#non-sysconfig-compatible-project-migration)
    for information about migrating to other MSPM0 devices.
    
    ## Example Usage
    
    Connect UART_RX and UART_TX or I2C_SDA and I2C SCL with the BSL Host (any microcontroller with UART/I2C respectively).
    Compile, load the example.
    Create BSL invocation condition using BSL Invoke pin or any other invocation methods.
    Send GetDeviceInfo command from the host.
    Device should respond back with the version information and SRAM buffer space available.
    Similarly Send erase, program, verification commands to program data in the memory.