This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2432: DLR effect RGMII receive packages.

Part Number: AM2432

Tool/software:

Hi

I am currently debugging the DLR function, using the SDK ind_comms_sdk_am2432x_09_02_00_08 and the ICSSG firmware in RGMII mode. I found that plugging and unplugging the network port when there is a DLR manager in the network will cause the network port to be unable to send packets and can only receive packets. This problem does not exist when there is no DLR data frame. The ethernetip_adapter_generic_device_rgmii_demo_am243x-evm_r5fss0-0_freertos_ti-arm-clang routine in the SDK is used. The same problem also occurs when running on EVM development board. I tried the MII mode routine on the development board and it is fine. Please help me see how to solve this problem.

Regards

Zekun