Part Number: TM4C123GH6PM
Tool/software:
Hi,
My if statement is causing a fault when a Timer0A interrupt is implemented (but not enabled yet). Whenever the below if-statement is checking if ADCvoltage is >= 939, it enters the FaultISR, but it works fine when I comment out the following code (Timer0Init and Timer0IntHandler) for Timer0A interrupt.
void Timer0Init(void){
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);
uint32_t ui32Period = (80000000/10);
TimerLoadSet(TIMER0_BASE, TIMER_A, ui32Period - 1);
// NVIC_PRI4_R = (NVIC_PRI4_R & 0x00FFFFFF) | (7 << 29);
IntEnable(INT_TIMER0A);
TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
IntMasterEnable();
TimerEnable(TIMER0_BASE, TIMER_A);
}
void Timer0IntHandler(void) {
// Clear the timer interrupt
TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
counter++;
if (counter == 1 | counter == 2) {
// Perform the action for 0.1 seconds
SPIWritePacket(0x10, 0x03, PrevChannelStatus | BUZZER_FAST_ON); // Buzzer (fast) On
PrevChannelStatus |= BUZZER_FAST_ON;
} else if (counter == 3) {
SPIWritePacket(0x10, 0x03, PrevChannelStatus & ~(BUZZER_FAST_ON)); // Buzzer (fast) On
PrevChannelStatus &= ~(BUZZER_FAST_ON);
} else if (counter >= 20) {
counter = 0; // Reset the counter every 2 seconds
}
}
SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); // System clock: 16*12.5/2.5 = 80MHz (MAX)
ui32PWMClock = SysCtlClockGet(); // PWM clock is SysClk
ui32Load = (ui32PWMClock / PWM_FREQUENCY) - 1; // Calculate load value
InitOE();
InitSPI();
InitADC();
InitUART();
InitPWM(ui32Load, 0); // Duty Cycle = 0 initially
MagneticInterlockTest();
OverrideTest();
while(1){
tempC = GetInternalTemp();
tempF = (1.8 * ulTemp_ValueC) + 32; // Celsius to Fahrenheit
ADCvoltage = GetVoltage(); // For solenoid lock
ambientTemp = GetTemp();
fanSpeed = GetFanSpeed();
IntToFloatVolt(ADCvoltage);
IntToFloatTemp(ambientTemp);
MagneticInterlockStatus = GPIOPinRead(GPIO_PORTC_BASE, GPIO_PIN_6);
OverrideStatus = GPIOPinRead(GPIO_PORTC_BASE, GPIO_PIN_5);
if(ADCvoltage >= 939){ // this causes fault // 939/4095 * 3.3 = 0.7567V (About 55V in a 1500V scale) // Voltage >= 55V
if(MagneticInterlockStatus & GPIO_PIN_6){ // Enclosure closed
if(OverrideStatus & GPIO_PIN_5){ // Override On (Enclosure was open & Override is enabled)
// Timer0Init();
////////////////////////////// omitted
}
What's the issue here?