Other Parts Discussed in Thread: RM48L950
Using a successfully installed Hercules RM48 USB Stick Development Kit, I imported the RM48 Hercules Demo into my ccs workspace to fix a bug and try downloading code. When I attempt to debug the project, the flash load begins (I can see the JTAG LED flashing) but fails with:
CortexR4: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
CortexR4: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x7ff0
CortexR4: Warning: (Error -1003 @ 0x2BC5) Internal error: Invalid parameter passed to function. Restart the application. If error persists, please report the error. (Release 5.0.429.0)
Cannot write to target
Is my board defective, or is there something I've overlooked?
-- e