Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2432: PCIe BAR Configuration on API Reference

Part Number: AM2432

Tool/software:

Hi,

 

My customer has some questions about API reference of PCIe. Could you help to answer their questions below ?

 

Q1) What do the definitions of Bar Configuration mean ?

              There are the following definitions as Pcie_BarType.

                            PCIE_BAR_TYPE32 (32 bits BAR)

PCIE_BAR_TYPE64 (64 bits BAR)

              Do these 32 bits and 64 bits mean data transmission size per one time ?

 

Q2) Bar Configuration Setting Possibility

              Bar Configuration on Syscfg is different between each version of example.

  • 64bit cannot be set with mcu_plus_sdk_am243x_09_01_00_41.
  • 64bit can be set with mcu_plus_sdk_am243x_09_02_01_05.

Will it be possible to set 64bit on the next version ?

 

Q3) What is the default setting of Pcie_AtuRegionMatchMode ?

              There are two types of

  • PCIE_ATU_REGION_MATCH_MODE_ADDR
  • PCIE_ATU_REGION_MATCH_MODE_BAR

              Which mode is set as default ?

 

Q4) BAR Number Setting

              On the Syscfg GUI, Inbound/Outbound can be set.

              How can they set a corresponding BAR number ?

 

Thanks and regards,

Hideaki

  • Hi Hideaki,

    Thanks for your query.

    PCIE_BAR_TYPE32 (32 bits BAR)

    • 32-bit base address field.

    PCIE_BAR_TYPE64 (64 bits BAR)

    • 2 contiguous BARs are combined to form a 64-bit prefetchable BAR.
    64bit can be set with mcu_plus_sdk_am243x_09_02_01_05.

    Q2-Q4:

    Which example you are referring here?

    Can you please help me with background of your end goal or use case?

    Regards

    Ashwani

  • Hello Hideaki,

                                PCIE_BAR_TYPE32 (32 bits BAR)

    PCIE_BAR_TYPE64 (64 bits BAR)

                  Do these 32 bits and 64 bits mean data transmission size per one time ?

    these refer to 32-bit vs. 64-bit wide BAR registers. A 64-bit BAR can be located anywhere in the PCIe address space, a 32-bit BAR needs to be located below 4GB.

    Bar Configuration on Syscfg is different between each version of example.

    • 64bit cannot be set with mcu_plus_sdk_am243x_09_01_00_41.
    • 64bit can be set with mcu_plus_sdk_am243x_09_02_01_05.

    Will it be possible to set 64bit on the next version ?

    09.02.01.05 is the first version to include the extended PCIe EP driver. I can't see why this would be dropped in upcoming versions.

    There are two types of

    • PCIE_ATU_REGION_MATCH_MODE_ADDR
    • PCIE_ATU_REGION_MATCH_MODE_BAR

                  Which mode is set as default ?

    That is a left-over in the API from previous controllers and not used within the driver. You can match incoming transactions only to BARs in EP mode.

    Q4) BAR Number Setting

                  On the Syscfg GUI, Inbound/Outbound can be set.

                  How can they set a corresponding BAR number ?

    The "Region Index" determines the BAR number.

    Regards,

    Dominic

  • Thanks Dominic for inputs.

    Hideaki Matsumoto, 

    Do you need further help here?

    Regards

    Ashwani