This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL2-TMS57012: CortexR4

Part Number: LAUNCHXL2-TMS57012

Tool/software:

I'm having some trouble using the bootloader project 6.1. Project 0 — Hercules Safety MCUs Documentation on the LAUNCHXL2-TMS57012

It was working fine for a while. But after running it several times, I started getting the following error messages as I was trying to step through the following function. 

This message popped up after line 94.

In addition, this error initially started popping up after I tried stepping over line 104. But after trying to debug the error, it started popping up after line 101, then line 94. It seems like the program is having a hard time reading the memory block with the actual instructions of the function.

I also know it is probably not a hardware issue as I tried with an old and a new board and got the exact same issue on both.