Tool/software:
Does lp-am243x m4-core support real time access? I failed to connect hardware while using M4-core. But when creating project it's connecting properly (xds).
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Does lp-am243x m4-core support real time access? I failed to connect hardware while using M4-core. But when creating project it's connecting properly (xds).
Hi,
for AM243Xtm LaunchPad: I'm using mcu_plus_sdk_am243x 08.06.00.43 and after it does not work i also try with version 09.02.00.50. I just started working with the TI board. If I made any mistakes, please excuse me. when I try with the M4, I don't get any errors while creating the project. I load the .out file and It connects to the hardware via XDS. However, when I try to run the GUI, it says "hardware not connected" Also, Previously, I was trying with the R5 cores. I couldn't establish a USB/UART connection. After the "waiting for data..." warning, it would time out, and I didn't understand what data it was waiting for. But it works with XDS. Thank you very much for your quick response.



Hello Hayriye,
Can you please also tell us which version of CCS Studio are you using?
Regards,
Tushar
Hi Hayriye,
Thanks for providing the above details.
Can you please confirm have you initialized the EVM properly?
To initialize the EVM with SBL binaries, please refer EVM_FLASH_SOC_INIT.
Regards,
Tushar
Hi Hayriye,
Thanks for the above confirmation.
I can see the above screenshot shared looks different than the usual CCS GUI.
I have tried to load and run the example from CCS v12.7.1 and I am able to successfully run the program without any errors.
Please refer below video.
To know more using CCS with MCU+SDK, please refer CCS_SETUP
Regards,
Tushar
Hi Tushar,
I think there are some misunderstanding. I am able to debug my code in CCS. I ask about Gui Composer. And pictures that i share is belong to gui composer interface.