This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi
I want to make non-sysconfig based CCS project.
I tryed deleate all sysconfig from SDK empty project.
But there is unknown error maybe generated by Linker.
May I have advices for resolve errors?
20240724_Empty_MSPM0G3507_TIclang.zip
best regards,
GR
Coming from the opposite direction: I used these steps to create an "Empty-G3507" project from the "Empty (with main)" project. [Bare-bones, no driverlib.]
1) Copy these files into the project:
C:\ti\mspm0_sdk_2_01_00_03\source\ti\devices\msp\m0p\linker_files\ticlang\mspm0g3507.cmd C:\ti\mspm0_sdk_2_01_00_03\source\ti\devices\msp\m0p\startup_system_files\ticlang\startup_mspm0g350x_ticlang.c
2) Add these to "Build Settings->Build->Compiler->Include Options":
C:\ti\mspm0_sdk_2_01_00_03\source C:\ti\mspm0_sdk_2_01_00_03\source\third_party\CMSIS\Core\Include
[The path prefix is of course the install directory for the SDK. Maybe there's a CCS/Eclipse wizard in the audience who can remind me how to add environment variables.]
3) Add this to main.c:
#include <ti/devices/msp/msp.h>
4) [optional] Add this to main():
GPIOA->GPRCM.PWREN = (GPIO_PWREN_KEY_UNLOCK_W | GPIO_PWREN_ENABLE_ENABLE);
[This just checks to see if I forgot anything. I think it's valid on any MSPM0.]
Hi Brian, Bruce,
Thanks for your information.
In my PC, If make project by CCS there is linker error that can't access own project folder.
So I will use the empty_non_sysconfig.
Best regards,
GR