Part Number: MSPM0G3505
Other Parts Discussed in Thread: LP-MSPM0G3507, SYSCONFIG
Tool/software:
Hi TI,
I need to use the UART-CAN bridge application.
I want to use the MSPM0G3505SRHBR (VQFN-32pin).
1-) Is it easy to migrate the project from MSPM0G3507SPMR (LQFP-64pin) to MSPM0G3505SRHBR (VQFN-32pin) MCU?
2-) The GPIO used for the UART-CAN bridge on the UART side are PA10(TX) and PA11(RX), right?
3-) I don't need analog pins. I can eliminate in my design R3 and C8 from LP-MSPM0G3507 (R3 connected to PA21_VREF- and C8 connected to PA23_VREF+), right?
4-) Can I use the crystals: SF32WK32768D31T002 and K2B400000810 with external 22pF capacitors? I attach the schematic and the crystals link.

SF32WK32768D31T002 TKD | C271654 - LCSC Electronics
K2B400000810 KYX | C2835990 - LCSC Electronics
Thanks very much. Best Regards.