Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TMS570LC4357: A tool to decode FEE blocks for failure analysis

Part Number: TMS570LC4357

Tool/software:

FEE data block decoder

  • https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/908/FEE_5F00_Decoder.exe

    PC command line executable file that interprets the FEE data saved by code composer and creates a readable output. By default the output is printed to the screen but it can be redirected to a file.

    Example: FEE_Decoder 2 0x4000 file.dat 1 >file.txt

    • First argument is number of virtual sectors (2 - 4)
    • Second argument is the size of a single virtual sector in 0x hex format
    • Third argument is the name of the input file created from Code Composer
    • Fourth argument is the number of DATASELECT bits, if omitted 0 is assumed
    • In this example the output is redirected into the file “file.txt”

    Please use Code Composer Studio to save the TMS570Lx or RM4x/RM5x bank 7 data images in a .dat file. For example to dump FEE 0, use the following:
    “Tools” -> “Save Memory”, File Type = “TI Data”; ->“NEXT”; Format = “32-Bit Hex – C Style”; Start Address = “0xF0200000”; “Specify the number of memory words to read” = “0x2000”; “Finish”