Part Number: MSPM0G3507
Tool/software:
[0]**** Build of configuration Debug for project i2c_to_uart_bridge_LP_MSPM0G3507_nortos_ticlang **** [1]"C:\\ti\\ccstheia141\\ccs\\utils\\bin\\gmake" -k -j 8 all -O [2]gmake[1]: 'i2c_to_uart_bridge_LP_MSPM0G3507_nortos_ticlang.out' is up to date. [3]**** Build Finished *
Build appears to be successful? Now I want to see how much memory was used. I use "memory Allocation" and get
Project 'i2c_to_uart_bridge_LP_MSPM0G3507_nortos_ticlang' ℹ️ The project must be successfully built first.
I am confused. I think I successfully built it. I get one mysterious "info" message during build which is "User must select a device after migration. User must make sure to select the same device as the CCS Launch Device setting for proper configuration.". I assume the severity of messages goes info, warning, error so surely a "info" message would not break the build?