Part Number: MCU-PLUS-SDK-AM243X
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi team,
We are currently using a custom flash with the AM243x Launchpad. During debugging, I'm encountering the following error:
MAIN_Cortex_R5_0_0: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x40: (Error -1065 @ 0x40) Unable to access device memory.
MAIN_Cortex_R5_0_0: File Loader: Verification failed: Target failed to write 0x00000000.
I suspect that the issue might be related to the linker command file configuration. Specifically, if we are using a custom flash, we need to change the address of the memory region in SysConfig.
Could anyone provide guidance on how to correctly configure the memory regions in SysConfig for our custom flash?
Regards,
Abinaya