Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello,
Is it possible to use the MSPM0 internal comparator outputs as the Quadrature Encoder Phase A and Phase B source for TIMG8 using the QEI mode?
I recognize that I could configure the comparator to output the result to a GPIO pin which could then be routed with a PCB trace to one of the TIMG8 capture GPIO's but I would rather route the signals internally if possible.
Is it possible to route the signals internally?
Thanks,
Ben