Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0C1104: Question about blocking

Part Number: MSPM0C1104

Tool/software:

Code Composer Studio -> Version: 12.7.1.00001

SDK -> mspm0_sdk_2_01_00_03

Hello,

I'm trying to block MSPM0C1104

So, I'm using the LP-MSPM0C1104 LaunchPad, and I also have a XMSM0C1104SRUKR WQFN 20 in my project.

I've tested both, in my Project and in the LaunchPad.

I'm getting a Time Out error when I enable “Erase MAIN and NONMAN necessary sectors only (see warning above)”

First I reset the DSSM


And configure the micro like this:

When I record the program it gets stuck at 0 and gives a Time Out error

When running it again it seems to have blocked but it does not load my firmware

I think I might be doing something wrong by locking the microcontroller