Part Number: AM2432
Tool/software:
Are all protocol in the SDK can be used for production without technical limitation, such as timeout, reset, etc....
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2432
Tool/software:
Are all protocol in the SDK can be used for production without technical limitation, such as timeout, reset, etc....
Hi Tony,
Yes all protocols and their corresponding examples that are present in the SDK can be directly used for production without any technical limitation.
Please take special care of board number while purchasing the device. For reference, consider the below device with the part number.
XAM6442B
SFGHAALV
Currently all the protocol stacks only work if the feature "F" (bold letter in part number) is present in the device. Please refer to the features in 9.1.2 section of the below document for more details.
www.ti.com/.../am2434.pdf
Additional point regarding EtherCAT protocol, customers will need to rebuild the Beckhoff stack library post getting the sources from ETG to remove any timeout related issues.
Regards,
Laxman