Part Number: MSPM0G3507
Tool/software:
Hello everyone,
I'm experiencing an issue with the MCU lp-MSPM0G03507 and I hope someone here can help me out. The problem is with the ADC channels, specifically the following:
- A0_1, which corresponds to PA26
- A1_4, which corresponds to PB17
- A1_7, which corresponds to PA21
I have connected a potentiometer to each of these channels, and I'm encountering the following issues:
- A0_1 (PA26): When the potentiometer value drops close to zero, the MCU shuts down completely, as if I had unplugged it.
- A1_4 (PB17): The channel behaves as if nothing is connected to it.
- A1_7 (PA21): As soon as I connect the potentiometer, the MCU shuts down immediately.
Has anyone experienced similar issues with these ADC channels?
Best regards,
Ali