Part Number: MSPM0G3507
Tool/software:
Hello,
I am working on MSPM0 controller.
For this i need to work on driver development.
So which tool is comfortable for beginner.
Please send me tool like
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSPM0G3507
Tool/software:
Hello,
I am working on MSPM0 controller.
For this i need to work on driver development.
So which tool is comfortable for beginner.
Please send me tool like
The standard tool is Theia.
For the firmware development, we recommend CCS Theia as Keith mentioned. For test hardware we recommend the LP-MSPM0G3507, which has a debugger included so you can simply plug the device into your PC and start testing firmware with CCS Theia.
Thanks Dylan OBrien and Keith Barkley for your suggestion.
i have MSPM0G3507 custom board and we are flashing .hex file using XDS11 Debugger and for debugging same.
So Theia tool support for this debugger?
Usually i am using IAR embedded for same controller.
But i have to install on my personal laptop, so that i am checking any alternate tool option.
Thanks and Regards,
Rohit Patil
You can use the XDS110 alongside CCS Theia.
If you are in the prototyping phase I would highly recommend utilizing the LP-MSPM0G3507 for software development, as this will help you rule out hardware issues when working on your code. However your set up should work fine as well.
After installing i didnt get any error but while creating new project getting below popup,
could you please help me for that?

Which version of CCS Theia are you using? That looks like an issue with TI Cloud Agent, which should be installed when you install CCS Theia. If you haven't installed CCS Theia recently you may just need to reinstall. However to be clear this issue is unrelated to the use of the XDS110.