Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1228-Q1: A few questions

Part Number: MSPM0L1228-Q1

Tool/software:

See questions from customer related to M0L1228 project.

  1. Can the timer count register be read reliably while the counter is running? We often use a free-running timer for timestamps. Some timers on some MCUs do not support reading the current counter value while the timer is running.

 

  1. How is a 32 bit read of TIMG12 or TIMG13 performed? The counter value register only has a 16 bit value and the function to read the register enforces a 16 bit read. I’m assuming two 16 bit reads need to be performed.

 

  1. The S32K1 family of MCUs have a small instruction cache. The BUS clock runs at a max of 48MHz and the CPU clock runs at a max of 80MHz. Also, writes to peripherals are buffered. For all these reasons, there is a need for what is termed Data Serialization. It is necessary to ensure a write to a peripheral completes before a dependent operation is performed. One method of enforcing Data Serialization is to read back the register just written to. The read won’t complete until the prior write does.
    1. Do the MSPM0L family of MCUs have a similar requirement for Data Serialization? So far it doesn’t seem like it.