Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi
May I have advice for my usecase?
I want to sync each TIMG countor without CPU interrupt.
So I want use generic event route (Subsciber and Publisher port) as sync signal.
And want to set if CC0 recieve subscibe event, generate TIMG countor reset(Load) .
but it is not works.
May I have advice?
I want to do as :
TIMG6 CC1 load event --> event route ID1 --> TIMG12 CC0 input source(IFCTL[0]) -> CC0 Compare event (countor = 1) --> CC0 generate Load event --> TIMG12 countor reset(Load)

I checked TIMG6 generate Load event in CCS debug mode.
(If connect generic route, Load event flag register can not see seted, maybe I think receiver clear flag automatically)
// clock divider
TIMG12->CLKDIV |= GPTIMER_CLKDIV_RATIO_DIV_BY_1; // div = /1, MCLK 80MHz
// clock source
TIMG12->CLKSEL |= GPTIMER_CLKSEL_BUSCLK_SEL_ENABLE; // TIMG6 bus clock is MCLK(80MHz). Please see Datasheet
//clock 2nd prescaler
TIMG12->COMMONREGS.CPS |= GPTIMER_CPS_PCNT_MASK & 0x00; // prescale /(8bit+1), dividing 1
// counter register
TIMG12->COUNTERREGS.CTRCTL = 0x00000000; // reset
TIMG12->COUNTERREGS.CTRCTL |= GPTIMER_CTRCTL_CVAE_ZEROVAL; // when module enabling, countor value set to zero
TIMG12->COUNTERREGS.CTRCTL |= GPTIMER_CTRCTL_CM_DOWN; // Count down mode
TIMG12->COUNTERREGS.CTRCTL |= GPTIMER_CTRCTL_REPEAT_REPEAT_1; // Repeat mode
TIMG12->COUNTERREGS.CTRCTL |= GPTIMER_CTRCTL_EN_DISABLED; // Timer counter disable
// load counter register, using full 16-bit
TIMG12->COUNTERREGS.LOAD |= 0x0000FFFF;
// event
// come from Channel ID1(TIMG6)
//FSUB_0 port
TIMG12->FSUB_0 |= (GPTIMER_FPUB_0_CHANID_MASK & 0x01); // connect channel ID1
// TIMG12->COUNTERREGS.IFCTL_01[0] |= GPTIMER_IFCTL_01_ISEL_FSUB0; //input source = FUSB_0
//setting of crosstriger
TIMG12->COMMONREGS.CTTRIGCTL |= GPTIMER_CTTRIGCTL_EVTCTTRIGSEL_FSUB0; //trigger from FSUB0
TIMG12->COMMONREGS.CTTRIGCTL |= GPTIMER_CTTRIGCTL_EVTCTEN_ENABLE; //input crosstrigger enable
TIMG12->COUNTERREGS.TSEL |= GPTIMER_TSEL_TE_ENABLED; // trigger enable
TIMG12->COUNTERREGS.TSEL |= GPTIMER_TSEL_ETSEL_TRIG_SUB0; // trigger from FSUB0
//setting CC0 imput source
TIMG12->COUNTERREGS.IFCTL_01[0] |= GPTIMER_IFCTL_01_ISEL_TRIG_INPUT; //input source = trigger
//setting CC0
TIMG12->COUNTERREGS.CC_01[0] |= (GPTIMER_CC_01_CCVAL_MASK & 0x1); // compare value
TIMG12->COUNTERREGS.CCCTL_01[0] |= GPTIMER_CCCTL_01_COC_CAPTURE; // capture mode
TIMG12->COUNTERREGS.CCCTL_01[0] |= GPTIMER_CCCTL_01_CCOND_CC_TRIG_RISE; //capture rising edge
TIMG12->COUNTERREGS.OCTL_01[0] |= GPTIMER_OCTL_01_CCPO_LOAD; // output load event
// Capture or Compare (CCP) setting
TIMG12->COMMONREGS.CCPD |= GPTIMER_CCPD_C0CCP1_OUTPUT; // TIMG12_CCP1 output
TIMG12->COMMONREGS.ODIS &= ~(GPTIMER_ODIS_C0CCP1_MASK); // CCP1 is output, not forced Low
TIMG12->COUNTERREGS.CC_01[1] |= (GPTIMER_CC_01_CCVAL_MASK & 135); // compare value
TIMG12->COUNTERREGS.CCCTL_01[1] |= GPTIMER_CCCTL_01_COC_COMPARE; // Compare mode
TIMG12->COUNTERREGS.OCTL_01[1] |= GPTIMER_OCTL_01_CCPIV_LOW; // initvalue = low output
TIMG12->COUNTERREGS.OCTL_01[1] |= GPTIMER_OCTL_01_CCPOINV_INV; // output is inversion
TIMG12->COUNTERREGS.OCTL_01[1] |= GPTIMER_OCTL_01_CCPO_FUNCVAL; // Output source = Signal generator value
TIMG12->COUNTERREGS.CCACT_01[1] |= GPTIMER_CCACT_01_LACT_CCP_LOW; // Load event = set Low
TIMG12->COUNTERREGS.CCACT_01[1] |= GPTIMER_CCACT_01_CDACT_CCP_HIGH; // Compare event = set high
// enabling clock
TIMG12->COMMONREGS.CCLKCTL |= GPTIMER_CCLKCTL_CLKEN_ENABLED; // clock enabled
//Before main roop
TIMG6->COUNTERREGS.CTRCTL |= GPTIMER_CTRCTL_EN_ENABLED; // Timer counter enable
TIMG12->COUNTERREGS.CTRCTL |= GPTIMER_CTRCTL_EN_ENABLED; // Timer counter enable
CC compare value is 0x1, so if there is recieved one event will generate compare event.
If it work as I think, TIMG12CC1output period must be same as TIMG6 PWM.
(Load value is TIMG12>TIMG6, so TIMG6 generate load event(=transmit as TIMG12 load event) before TIMG12 PWM priod. So each priod will be same)
Thanks,
GR