Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi TI Experts,
Customer is working on AM243x SDK9.2.
They have built the Tamagawa project, and the Tamagawa PRU-ICSS firmware is loaded and running successfully.
As you could see below, there is an option 9 to configure the IEP reset cycle count & IEP trigger time.
|------------------------------------------------------------------------------|
| Select DATA ID Code |
|------------------------------------------------------------------------------|
| 0 : Data readout, Absolute (Data ID 0) |
| 1 : Data readout, Multi-turn (Data ID 1) |
| 2 : Data readout, Encoder-ID (Data ID 2) |
| 3 : Data readout, Absolute & Multi-turn (Data ID 3) |
| 4 : Writing to EEPROM (Data ID 6) |
| 5 : Reset (Data ID 7) |
| 6 : Reset (Data ID 8) |
| 7 : Reset (Data ID C) |
| 8 : Readout from EEPROM (Data ID D) |
| 9 : Start periodic continuous mode |
|------------------------------------------------------------------------------|
|
| enter value: 9
| Enter IEP reset cycle count (must be greater than Tamagawa cycle time including timeout period, in IEP cycles):
| Enter IEP trigger time(must be less than or equal to IEP reset cycle, in IEP cycles):
Customer has the following 2 questions regarding to the configuration of the cycle time in option 9 above.
1: What is the unit of the IEP cycle? (for example, is it in microsecond us or millisecond ms or nanosecond ns)
2: Customer has tried enter the IEP trigger time to 50, but the result is only refreshed 1 time, not being continuously refreshed. Customer wants to know the reason why only 1 time the result is refreshed?
Could you help please provide some feedback for the above 2 questions please?
Thanks,
Kevin