Part Number: AM2434
Tool/software:
Hi,
My customer is now considering two chip solution for multi-axis servo control like below.
Device 1 (D1) : AM2434 for 3-axis <---- < FSI > ----> Device 2 (D2) AM2434 for 6-axis
Also, considering the secondary boot from D1 to D2 via FSI. Therefore, D1 must be start up earlier than D2.
In this case, D1 and D2 can be directly connected via FSI ? Should capacitor or switch be used to decouple before power up D2 ?
Also, is there any boot timing caution between D1 and D2 ?
Thanks and regards,
Hideaki