Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi TI experts,
I'm currently learning CAN communication using LP-MSPM0G3597.
I'm using the C:\ti\mspm0_sdk_2_01_00_03\examples\nortos\LP_MSPM0G3507\driverlib\mcan_single_message_tx example project.
The compiler I'm using is Code Composer Studio Version: 12.6.0.00008. After loading the program, it can be compiled and burned normally.
Following the example program's instructions, I pressed PB21 (S2 button) and used an oscilloscope and logic analyzer to measure,
but I found that PA12(CAN TX) and PA13(CAN RX) have no output. Could you please tell me what caused this?
Additionally, this example program demonstrates CAN FD mode transmission. If I want to change it to a general CAN 8-byte transmission mode,
how should I configure the syscfg file? Are there any relevant example programs and configuration files that you can provide?
I'm using SDK mspm0_sdk_2_01_00_03 and CCS 12.6.
Thank you!
Allen Yang