Part Number: AM2432
Tool/software:
MCU SDK: 9.02
Industry SDK: ind_comms_sdk_am243x_09_02_00_08
Issue: Enter Data Abort over 6 to 7 hours, or longer a litte.
Test on 8pcs boards, all triggered this issue. Did not notice the call trace before, but currently 3 pcs on debugging all triggered from same place from call trace.
From CCS, captured the trigger place and read out fault address (0x3220747A)

From the call trace, triggered the data abort inside LLDP_deleteNeighborDevice(), should be ldr instruction at 0x700DD6AC accessed invalid address, seems R0 passed in a illegal address, as this is inside the protocol, application did not call these functions directly. need BU help analysis.