Part Number: MSPM0G3507
Tool/software:
How to add CRC32 verification for firmware upgrades? I want to incorporate CRC32 verification as the final step in the upgrade process. Only if the verification is correct, the system can proceed to jump to the application to run. This measure is intended to prevent the firmware file from being corrupted, which could lead to erroneous upgrades and render the device unable to function or be upgraded properly.