Part Number: MSPM0G3507
Tool/software:
Dear TI,
We are using following MSPM0G3507 --> SDK 2.0.0.1 and CCS studio
We have develop our application code (In the same we are using ADC , CAN, TIMER for PWM , IC etc) on the above MCU, and the issue we are are facing is that when we run our application code without hardware board (in that all other hardware logic is implement like PI controller to current setting other things ) its working fine.
But as we power up the hardware board and MCU run for time after that MCU get halt (stop running). we check HARD_FAULT hander to reset the MCU but there is no hard fault triggering , even systick get stop.
We don't able to find the possible cause of the same,
Can you please let us know which things make the MCU halt , we checked the MCU voltage 3.3 and GND its also fine,
Best regards