Part Number: MSPM0G3507
Tool/software:
Hi experts,
Is it possible to exit standby mode with an instruction (like _BIC_SR_IRQ(CPUOFF); // Clear LPM from 0(SR) on an MSP430).
Thanks in advance.
/*
* Exit_Standby.c
*
* Created on: 7 août 2024
* Author: Test Team
*/
#include "ti_msp_dl_config.h"
volatile unsigned char RX_Data = 0;
int main(void)
{
SYSCFG_DL_init();
NVIC_ClearPendingIRQ(UART_0_INST_INT_IRQN);
NVIC_EnableIRQ(UART_0_INST_INT_IRQN);
DL_SYSCTL_enableSleepOnExit();
while (1) {
__WFI();
DL_GPIO_togglePins(GPIO_LEDS_PORT,
GPIO_LEDS_USER_LED_1_PIN | GPIO_LEDS_USER_TEST_PIN);
}
}
void UART_0_INST_IRQHandler(void)
{
switch (DL_UART_Main_getPendingInterrupt(UART_0_INST)) {
case DL_UART_MAIN_IIDX_RX:
RX_Data = DL_UART_Main_receiveData(UART_0_INST);
while (DL_UART_isBusy(UART_0_INST));
DL_UART_Main_transmitData(UART_0_INST, RX_Data);
if(RX_Data == "@")
{
// Exit standby mode only if RX car is "@"
}
break;
default:
break;
}
}