Part Number: TMDS243EVM
Tool/software:
Hi Ti Expert,
I'm trying to use 243EVM as RC and Intel FPGA as EP.
I can successfully read the Device ID and Vendor ID of the EP. Following the example C:\ti\mcu_plus_sdk_am243x_09_00_00_35\examples\drivers\pcie\pcie_buf_transfer\pcie_buf_transfer_rc
And I add the following Bar Configure function. Following the post: PCIe link up c6678 - Processors forum - Processors - TI E2E support forums
int32_t pcie_fpga_ep_bar1_cfg(Pcie_Handle handle)
{
int32_t status = SystemP_SUCCESS;
Pcie_BarCfg barCfg;
barCfg.location = PCIE_LOCATION_REMOTE;
barCfg.mode = PCIE_EP_MODE;
barCfg.base = 0x70000000;
barCfg.prefetch = PCIE_BAR_NON_PREF;
barCfg.type = PCIE_BAR_TYPE32;
barCfg.memSpace = PCIE_BAR_MEM_MEM;
barCfg.idx = 0;//1;
status = Pcie_cfgBar (handle, &barCfg);
//DebugP_assert(SystemP_SUCCESS == status);
if (SystemP_SUCCESS != status)
{
DebugP_log("FPGA Bar1 configure fail\r\n");
}
else
{
DebugP_log("FPGA Bar1 configure done\r\n");
}
return status;
}
This picture is the configure of FPGA and my Outbound.


My program always stuck here in Pcie_readRegs():

please help me about it.
Thanks
Chunyang