Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: Bootstrap configuration for RMII in Dp83822

Part Number: AM2634

Tool/software:

Dear Team,

I want connect AM2634 with 2 parallel phy (DP83822) on RMII (100 mbps) connected on same MDIO/MDC (N16,M17)

On a copper connection So i required the boot strap configurations required to make it run.

Mode - 100mbps full duplex

RMII master mode 

Do we need to assign different address for each phy?

  • Hi Vikas,

    I have re-assigned the query to our PHY experts. They will get back in a few hours in California time.

    Best regards,
    Shaunak

  • Hi Vikas!

    I'm an Applications Engineer from the Ethernet PHY team can gladly assist with this query. 

    To answer your question, yes, both PHYs can be connected to the same MDC/MDIO bus and will require a unique PHY Address.

    Regards,

    Alvaro

  • thanks for reply, i have few more questions, please give your feedback

    Requirements
    PHY1 Address 0x0000
    PHY2 Address 0x0011
    Mode of Operation  100BASE-TX, Full-Duplex, Auto-MDIX
    LED0 Configuration Blink Tx/Rx Activity
    LED1 Configuration ON for 100 Mbps SPEED
    MAC configuration  RMII Master

    Required information 
    Pins PU/PD Strap mode Value
    COL      
    RX_D0      
    Rx_D1      
    Rx_D2      
    Rx_D3      
    LED0      
    LED1      
    CRS      
    Rx_ER      
    Rx_DV      

    Please fill above blank space

    Aditional Questions
    1. Can we saparate link and Tx/Rx leds
    2. Will speed led work in auto MDIx mode
    3. How to enable auto negotiation