Part Number: TMDSCNCD263
Tool/software:
We have the TMDSCNCD263 and the control card base board. Is it possible to use UART2? If so, what settings need to be setup to enable it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSCNCD263
Tool/software:
We have the TMDSCNCD263 and the control card base board. Is it possible to use UART2? If so, what settings need to be setup to enable it?
Hi Tom,
To use UART2, you will need to configure the device pinmux for the UART2 peripheral.
For simplicity, I am going to demonstrate this using the Empty SDK example, but this can be configured in any CCS project.





You can now use UART2 on the EVM.
Regards,
Brennan
Unfortunately, we found it requires a bit more work. The resistor network RA2 must be depopulated, and the network RA3 must be populated to rout the signals out.
Tom,
Yes, that is also correct. To make the resistor swap easier, I suggest depopulating RA2 and then solder bridging the pads on the RA3 footprint.
Regards,
Brennan