Part Number: AM2432
Tool/software:
Hello Expert,
I'm encountering an issue with test number 133 (R5FSS0_CORE0_INTR_IN_133) while testing:
In the program, enabling interrupt 133 on R50_0 core and registering a callback function works fine during normal loading. However, after performing a System Reset using CCS (whether it's at any time), upon re-loading the program and enabling the interrupt, it repeatedly enters the interrupt callback function instead of proceeding with the subsequent program execution. The issue resolves when we perform a power reset.
My test code is based on modifications made to the hello world example routine; there are no other operations involved.
void call(void *args)
{
DebugP_log("callback\r\n");
}
void hello_world_main(void *args)
{
/* Open drivers to open the UART driver for console */
Drivers_open();
Board_driversOpen();
HwiP_Params hwiPrms;
HwiP_Object cmpHwiObject;
/* Register pin interrupt */
HwiP_Params_init(&hwiPrms);
hwiPrms.intNum = 133;
hwiPrms.priority = 1U;
hwiPrms.callback = &call;
hwiPrms.isPulse = 0;
HwiP_construct(&cmpHwiObject, &hwiPrms);
DebugP_log("Hello World!\r\n");
}Could you please help me analyze what might be causing this problem?
Thank you,
Best regards
Jimmy