Part Number: TMS570LS3137
Tool/software:
Dear support team,
I am trying to run the TCP/ UDP client server code based on lwip on my laptop.
I have installed the lwip library for linux and compiling the code using this. Somehow it always compiles , but on running the executables, I do not see any output.
The idea is that, if I am able to compile it and run on my local system, I can understand the flow better and proceed with integrating it on the TI MCU.
I have attached my entire folder and also the file with details regarding how I have configured.
My question is whether running the lwip based programs on LINUX is even possible or not ? Is there any restrictions that it will only work on microcontrollers ? Is there any specific configuration to be made? Any additional interfaces to be created?
On my MCU it is working completely fine, but i wish to have it up and running on the laptop too.
Any help in this regard would be highly appreciated.
The link to the resources is below
Thank you in advance !
Chandana.