Part Number: MSPM0L1304
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
I see that with the BSL you can read the "application version" with the "Device Info" command. What I do not find is how to set the this version in my application in the flash area. Is there an example available or a documentation?
"The BSL supports returning an application version number through the BSL serial
interface. This allows the BSL host to interrogate the firmware version without
being able to read the firmware. The version field is 32 bits in length.
To link the application version command to a version number programmed in the
main flash, program the address of the version number in this field.
The version data is only returned if the specified address corresponds to a
valid flash memory address."
--
Heiko